Part Number: LMH0070
Tool/software:
In the POWER UP chapter of Datasheet P9, There is a description as "both power supplies are brought up."
When "both power supplies are brought up." means, How many voltages are required for 2.5V and 3.3V?
(Is there no problem if the value is within the range of "Recommended Operating Conditions"?)
And If Power off and Power on suddenly, there is a concern that the 2.5V and 3.3V may not drop enough.
In such a case, Are there any specifications stating how low 2.5V and 3.3V must be?
If this specification is not met, what will be the impact on the LMH0070?