Part Number: TPS62932
Tool/software:
Buck Switching Regulator team,
We have a customer designing with TPS62932, and the switching frequency must be 1 MHz or higher. The application is extremely cost sensitive.
If the switching frequency is set to 1.0 MHz, there's a 20kOhm resistor pull down on the Rt pin.
If the switching frequency is set to 1.2 MHz, there's no pull down resistor on the Rt pin. It is tied to ground.
Setting to 1.2 MHz saves the cost of the resistor. It reduces the efficiency very slightly, based on Webench. Other than efficiency, can you think of any negative effects of operating at 1.2MHz?
Thanks,
Darren