Part Number: DP83848I
Tool/software:
Hi Team,
The customer would like to switch the mode from fixed 100Base-T to fixed 10Base-T without power cycle.
They changed the register settings with the following procedure, but it didn't switch.
Could you tell me the correct procedure?
1) At power up, set Bit13=1, Bit8=1 in the BMCR (Basic Mode Control Register); 100Mb/s, Full duplex
2) Set Bit15=1 in the BMCR; Reset
3) Set Bit13=0, Bit12=0, Bit9=0 in the BMCR, and set Bit8=1; Auto-Negotiation Disabled, 10Mb/s, Full duplex
Best Regards,