Part Number: THVD8000
Other Parts Discussed in Thread: THVD8010
Tool/software:
Hi
AC line PLC communication is being implemented using THVD8000
1. Problem: Noise is recognized as carrier when communicating using AC line and the UART bit is broken (see white box below)
2. Contact:
A. How many carrier waves are recognized as signals when modulating OK?
B. Sounds good, carrier recognition method?
i. Is it only recognized at the voltage level? (e.g. above 200 mV it is recognized as a carrier.)
ii. Do you recognize it as SNR above a certain level?
3. Request
A. Is there any way to improve misrecognition due to power noise and switching noise?

Thanks