Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN11623-Q1: BMS

Part Number: TCAN11623-Q1

Tool/software:

Hello Experts,

We are using TCAN11623DMTRQ1 ass our primary CAN trans receiver in our 400V & 48V BMS Project. Where it is powered by 12V and VIO-is 3.3V. During Bulk Current Injection test at LEVEL 3 (150mA at 10Mhz to 400 MHz), we are facing a constant failure of CAN data loss mostly around 15Mhz.For your reference, I am Attaching the schematics for your review. Please share your point of view on that or any suggestion.

Thanks,

  • Abhiram,

    Apologies for the significant delay. Is it possible to share any waveforms during the test? Your schematic looks ideal, the only addition I would recommend are filter capacitors on both CANH and CANL pins, but given those would be better for high frequency, they won't help much with a lower frequency failure.

    But yes, please share CANH, CANL, and RXD during the testing so we can understand how exactly the communication is failing.

    Regards,

    Eric Hackett