Part Number: DS15BR400
Tool/software:
Hi,
I am using 4-channel LVDS buffer IC DS15BR400, I am using only 2 channels.
Un-used channels should be left floating or should terminate to ground?
Regards,
Pawan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The unused inputs should be tied off as listed below to ensure the outputs remain in a stable state.
IN+ = 3.3K to VDD
IN- = 3.3K to GND
This will ensure 50mV of offset at the input which is enough to keep the output from switching.
Thanks
David