Part Number: ULC1001-DRV290XEVM
Other Parts Discussed in Thread: ULC1001, USB2ANY
Tool/software:
Hello everyone,
I have a issue with the GUI of ULC1001. I start the programm and deactivate the demo mode by removing the hook. Then config is loading, after a few seconds the following message appears:
“Error -5 occurred at Error Converter (Err Code or Status).avi
Possible reason(s):
Transmit failed
Complete call chain:
Error Converter (ErrCode or Status).vi
U2a I2C Internal read.vi
ULC1001 Device Interface.lvclass:Read Register.vi
ULC1001 Device Interface.lvclass:Read faults.vi
ULC1001.lvlib:Main.vi”
I can press only exit and the GUI shuts down.
Can someone help? The USB device has the newest firmware and the USB2ANY device was already exchanged and is completly new.
Kind regards,
Fabian