Part Number: DS320PR1601
Tool/software:
Do TI PCIe redrivers support bifurcation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, TI's PCIe Gen4 and Gen5 redrivers inherently support bifurcation, as these devices work on the electrical level only.
Note that for x4, x8, or x16 applications, device PD pins can be used to control device power down and RX Detect functionality.
For x2 applications, please refer to the following FAQ for further details: [FAQ] DS320PR1601: Receiver Detect Reset for x2 SSD Hot Plug Applications
Best,
David