Other Parts Discussed in Thread: TCA9517, , TCA9416
Tool/software:
Dear Specialists,
My customer is evaluatingP82B96 and TCA9517, communication is not possible.
I would be grateful if you could advise.
---
When I connect the Sx and Sy of the P82B96 to the B side of the TCA9517, communication is not possible.
The GND level at that time rose to 0.8V.
I wonder if the reason it doesn't work is because I connected a device with a buffer function in series.
Could you please introduce a device that can be used instead of the TCA9517.
On the other hand, when I directly connect a 3.3V compatible I2C sensor device to the P82B96,
it works without any problems. (Temperature sensor, acceleration sensor, pressure sensor, etc.)
The GND level does not float.
---
I appreciate your great help in advance.
Best regards,
Shinichi