This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1146-Q1: WUF data validation with 2 data bits

Part Number: TCAN1146-Q1

Tool/software:

HI BU team 

In the TCAN1146-Q1 WUF data validation process, 8 data bytes are implemented and data mask is enabled  by the customer. Customer wanted that TCAN1146-Q1 can be waked-up only when there are 2 data bits matching between the received frame data and configured  frame data. Can TCAN1146-Q1 support this requirement? If yes, would you show how TCAN1146-Q1 are configured to implement it in details?

The background is from autosar can network management. ONLY both PNI and PNC bits are matched then TCAN1146-Q1 can be selected waked-up.

Thanks