Part Number: TCA9803
Tool/software:
Hi team,
I would have a question regarding the TCA9803.
Would it be possible to use this device as a buffer for 1.8V, but also to change the input impedance from example 2.2k Ohm at the input to 100k Ohm at the output?
Something like this:

It would be important for the end device to see 100k Ohm.
Would this be possible with TCA9803 or do do you have other suggestions in order implement such a solution?
Best regards,
Rosario