Part Number: TCA6408A
Other Parts Discussed in Thread: TCAL6416, TCAL9539
Tool/software:
Hi,
May I know there have 2 x open drain INT I/O Expander solution.
I found most of I/O Expander only have 1 x open drain INT.
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
No I2C IO expander in our portfolio has more than 1 interrupt.
The /INT pin is set when any of the IO's configured as INPUTs change from their original state.
In some I2C Io expanders such as TCAL9539 or TCAL6416, these devices have an interrupt status register that identifies which IO trigger the interrupt on the /INT pin. This helps to determine which IO was the cause of the interrupt.
Regards,
Tyler