Part Number: DS125DF1610
Tool/software:
In the datasheet https://www.ti.com/lit/gpn/ds125df1610 page 21. It mentioned:
A full eye diagram capture can be performed when the CDR is locked. The eye diagram is constructed within a
64 x 64 array, where each cell in the matrix consists of an 16-bit word. Users can manually adjust the vertical
scaling of the EOM or allow the state machine to control the scaling which is the default option. The horizontal
scaling controlled by the state machine and is always directly proportional to the data rate.
When a full eye diagram plot is captured, the retimer will shift out 4 16-bit words of junk data that should be
discarded followed by 4096 16-bit words that make up the 64 x 64 eye plot. The first actual word of the eye plot
from the retimer is for (X, Y) position (0,0). Each time the eye plot data is read out the voltage position is
incremented. Once the voltage position has incremented to position 63, the next read will cause the voltage
position to reset to 0 and the phase position to increment.
In SigCon, I see negative voltage in the plot, and I change EOM_SEL_VRANGE, and find the eye shows on the very negative side. Please find the same signal with different setting below.
EOM_SEL_VRANGE = 100mV

EOM_SEL_VRANGE = 200mV

EOM_SEL_VRANGE = 300mV

EOM_SEL_VRANGE = 400mV