Part Number: DP83TG720S-Q1
Tool/software:
Hello,
The DP83TG720S- Q1 uses functional pins as strap options to place the device into specific modes of operation. For PHY address, 3 level are necessary.
In my setup, I noticed that address which require Mode 3 [ ie Adress (5),(10),(13),(14) and (15) ], obtained when RH equal to 800 Ohm for VDDIO 1V8, is problematic.
The communication and so the configuration fail. At reset, the voltage is well above 0.84*VDDIO ( 1V512 ) as mentioned in your electrical characteristics ( around 1V6 measured ).
I changed the value of RH in order to get a higher voltage ( ie 1V7 ) and the PHY is now configured properly !!!!
Note that I designed a Ethernet module board with your chip on board and on some module the PHY works properly for all address with the RH value mentioned in the datasheet.
Could you help me on this topics ? are you aware on this problem ?
Is it ‘normal’ that I have to change the RH value ?
Thanks in advance for your reply.