Part Number: PCA9515A
Other Parts Discussed in Thread: PCA9515B, , TCA9800, TCA9509, TCA9517
Tool/software:
Hi,
Could you tell me the newer recommendation device against PCA9515ADR?
BR,
Taku
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The web site recommends the PCA9515B, but it is not available in the SOIC package.
The PCA9515x has a static voltage offset on both sides. Newer devices like the TCA9517(A) or TCA9509 have an offset only on one side, which is usually preferred (but it does not make a difference in existing circuits that already work with the PCA9515A). The TCA9800/1/2/3 uses a current source instead of a voltage offset, which canresult in better signal quality, but you must not use pull-up resistors on the B side.