Part Number: DP83TC812R-Q1
Tool/software:
Dear sir.
Our team has purchased phy chip for dp83tc812 from ti, but I have some problems when I am using the driver file for dp83tc812 under linux written by you. The details are as follows
We are under linux system based on linux4.19 kernel install petalinux software for driver module add but when using the driver code you pro
// SPDX-License-Identifier: GPL-2.0
/*
* Driver for the Texas Instruments DP83TC812 PHY
*
* Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
*
*/
#include <linux/ethtool.h>
#include <linux/etherdevice.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>
#include <linux/netdevice.h>
#define DP83TC812_CS1_0_PHY_ID 0x2000a270
#define DP83TC812_CS2_0_PHY_ID 0x2000a271
#define DP83TC813_CS2_0_PHY_ID 0x2000a211
#define DP83TC814_CS2_0_PHY_ID 0x2000a261
#define DP83812_DEVADDR 0x1f
#define DP83812_DEVADDR_MMD1 0x1
#define DP83812_STRAP 0x45d
#define MII_DP83812_SGMII_CTRL 0x608
#define MII_DP83812_RGMII_CTRL 0x600
#define MII_DP83812_INT_STAT1 0x12
#define MII_DP83812_INT_STAT2 0x13
#define MII_DP83812_INT_STAT3 0x18
#define MII_DP83812_RESET_CTRL 0x1f
#define DP83812_HW_RESET BIT(15)
#define DP83812_SW_RESET BIT(14)
/* INT_STAT1 bits */
#define DP83812_RX_ERR_CNT_HALF_FULL_INT_EN BIT(0)
#define DP83812_TX_ERR_CNT_HALF_FULL_INT_EN BIT(1)
#define DP83812_MS_TRAIN_DONE_INT_EN BIT(2)
#define DP83812_ESD_EVENT_INT_EN BIT(3)
#define DP83812_LINK_STAT_INT_EN BIT(5)
#define DP83812_ENERGY_DET_INT_EN BIT(6)
#define DP83812_LINK_QUAL_INT_EN BIT(7)
/* INT_STAT2 bits */
#define DP83812_JABBER_INT_EN BIT(0)
#define DP83812_POL_INT_EN BIT(1)
#define DP83812_SLEEP_MODE_INT_EN BIT(2)
#define DP83812_OVERTEMP_INT_EN BIT(3)
#define DP83812_FIFO_INT_EN BIT(4)
#define DP83812_PAGE_RXD_INT_EN BIT(5)
#define DP83812_OVERVOLTAGE_INT_EN BIT(6)
#define DP83812_UNDERVOLTAGE_INT_EN BIT(7)
/* INT_STAT3 bits */
#define DP83812_LPS_INT_EN BIT(0)
#define DP83812_WUP_INT_EN BIT(1)
#define DP83812_WAKE_REQ_INT_EN BIT(2)
#define DP83811_NO_FRAME_INT_EN BIT(3)
#define DP83811_POR_DONE_INT_EN BIT(4)
#define DP83812_SLEEP_FAIL_INT_EN BIT(5)
/* RGMII_CTRL bits */
#define DP83812_RGMII_EN BIT(3)
/* SGMII CTRL bits */
#define DP83812_SGMII_AUTO_NEG_EN BIT(0)
#define DP83812_SGMII_EN BIT(9)
/* Strap bits */
#define DP83812_MASTER_MODE BIT(9)
#define DP83812_RGMII_IS_EN BIT(7)
enum dp83812_chip_type {
DP83812_CS1 = 0,
DP83812_CS2,
DP83813_CS2,
DP83814_CS2,
};
struct dp83812_init_reg {
int reg;
int val;
};
static const struct dp83812_init_reg dp83812_master_cs1_0_init[] = {
{0x523, 0x0001},
{0x800, 0xf864},
{0x803, 0x1552},
{0x804, 0x1a66},
{0x805, 0x1f7b},
{0x81f, 0x2a88},
{0x825, 0x40e5},
{0x82b, 0x7f3f},
{0x830, 0x0543},
{0x836, 0x5008},
{0x83a, 0x08e0},
{0x83b, 0x0845},
{0x83e, 0x0445},
{0x855, 0x9b9a},
{0x85f, 0x2010},
{0x860, 0x6040},
{0x86c, 0x1333},
{0x86b, 0x3e10},
{0x872, 0x88c0},
{0x873, 0x0003},
{0x879, 0x000f},
{0x87b, 0x0070},
{0x87c, 0x003f},
{0x89e, 0x00aa},
{0x523, 0x0000},
};
static const struct dp83812_init_reg dp83812_master_cs2_0_init[] = {
{0x523, 0x0001},
{0x81C, 0x0fe2},
{0x872, 0x0300},
{0x879, 0x0f00},
{0x806, 0x2952},
{0x807, 0x3361},
{0x808, 0x3D7B},
{0x83E, 0x045F},
{0x834, 0x8000},
{0x862, 0x00E8},
{0x896, 0x32CB},
{0x03E, 0x0009},
{0x01f, 0x4000},
{0x523, 0x0000},
};
static const struct dp83812_init_reg dp83812_slave_cs1_0_init[] = {
{0x523, 0x0001},
{0x803, 0x1b52},
{0x804, 0x216c},
{0x805, 0x277b},
{0x827, 0x3000},
{0x830, 0x0543},
{0x83a, 0x0020},
{0x83c, 0x0001},
{0x855, 0x9b9a},
{0x85f, 0x2010},
{0x860, 0x6040},
{0x86c, 0x0333},
{0x872, 0x88c0},
{0x873, 0x0021},
{0x879, 0x000f},
{0x87b, 0x0070},
{0x87c, 0x0002},
{0x897, 0x003f},
{0x89e, 0x00a2},
{0x510, 0x000f},
{0x523, 0x0000},
};
static const struct dp83812_init_reg dp83812_slave_cs2_0_init[] = {
{0x523, 0x0001},
{0x873, 0x0821},
{0x896, 0x22ff},
{0x89E, 0x0000},
{0x01f, 0x4000},
{0x523, 0x0000},
};
struct dp83812_private {
int chip;
bool is_master;
bool is_rgmii;
bool is_sgmii;
};
static int dp83812_read_straps(struct phy_device *phydev)
{
struct dp83812_private *dp83812 = phydev->priv;
int strap;
strap = phy_read_mmd(phydev, DP83812_DEVADDR, DP83812_STRAP);
if (strap < 0)
return strap;
printk("%s: Strap is 0x%X\n", __func__, strap);
if (strap & DP83812_MASTER_MODE)
dp83812->is_master = true;
if (strap & DP83812_RGMII_IS_EN)
dp83812->is_rgmii = true;
return 0;
};
static int dp83812_reset(struct phy_device *phydev, bool hw_reset)
{
int ret;
if (hw_reset)
ret = phy_write(phydev, MII_DP83812_RESET_CTRL,
DP83812_HW_RESET);
else
ret = phy_write(phydev, MII_DP83812_RESET_CTRL,
DP83812_SW_RESET);
if (ret)
return ret;
mdelay(100);
return 0;
}
static int dp83812_phy_reset(struct phy_device *phydev)
{
int err;
int ret;
err = phy_write(phydev, MII_DP83812_RESET_CTRL, DP83812_HW_RESET);
if (err < 0)
return err;
ret = dp83812_read_straps(phydev);
if (ret)
return ret;
return 0;
}
static int dp83812_write_seq(struct phy_device *phydev, const struct
dp83812_init_reg *init_data, int size)
{
int ret;
int i;
for (i = 0; i < size; i++) {
ret = phy_write_mmd(phydev, DP83812_DEVADDR, init_data[i].reg,
init_data[i].val);
if (ret)
return ret;
}
return 0;
}
static int dp83812_chip_init(struct phy_device *phydev)
{
struct dp83812_private *dp83812 = phydev->priv;
int ret;
ret = dp83812_reset(phydev, true);
if (ret)
return ret;
if (dp83812->is_master)
ret = phy_write_mmd(phydev, DP83812_DEVADDR_MMD1, 0x0834, 0xc001);
// ret = phy_write_mmd(phydev, DP83812_DEVADDR, 0x0834, 0xc001);
else
ret = phy_write_mmd(phydev, DP83812_DEVADDR_MMD1, 0x0834, 0x8001);
// ret = phy_write_mmd(phydev, DP83812_DEVADDR, 0x0834, 0x8001);
switch (dp83812->chip) {
case DP83812_CS1:
if (dp83812->is_master)
ret = dp83812_write_seq(phydev,
dp83812_master_cs1_0_init,
ARRAY_SIZE(dp83812_master_cs1_0_init));
else
ret = dp83812_write_seq(phydev,
dp83812_slave_cs1_0_init,
ARRAY_SIZE(dp83812_slave_cs1_0_init));
break;
case DP83812_CS2:
if (dp83812->is_master)
ret = dp83812_write_seq(phydev,
dp83812_master_cs2_0_init,
ARRAY_SIZE(dp83812_master_cs2_0_init));
else
ret = dp83812_write_seq(phydev,
dp83812_slave_cs2_0_init,
ARRAY_SIZE(dp83812_slave_cs2_0_init));
break;
case DP83813_CS2:
if (dp83812->is_master)
ret = dp83812_write_seq(phydev,
dp83812_master_cs2_0_init,
ARRAY_SIZE(dp83812_master_cs2_0_init));
else
ret = dp83812_write_seq(phydev,
dp83812_slave_cs2_0_init,
ARRAY_SIZE(dp83812_slave_cs2_0_init));
break;
case DP83814_CS2:
if (dp83812->is_master)
ret = dp83812_write_seq(phydev,
dp83812_master_cs2_0_init,
ARRAY_SIZE(dp83812_master_cs2_0_init));
else
ret = dp83812_write_seq(phydev,
dp83812_slave_cs2_0_init,
ARRAY_SIZE(dp83812_slave_cs2_0_init));
break;
default:
return -EINVAL;
};
if (ret)
return ret;
mdelay(10);
// phy_write_mmd(phydev, DP83812_DEVADDR, 0x523, 0x00);
/* Do a soft reset to restart the PHY with updated values */
return dp83812_reset(phydev, false);
}
static int dp83812_config_init(struct phy_device *phydev)
{
int value, err;
err = dp83812_chip_init(phydev);
if (err)
return err;
value = phy_read_mmd(phydev, DP83812_DEVADDR, MII_DP83812_SGMII_CTRL);
if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
err = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_SGMII_CTRL,
(DP83812_SGMII_EN | value));
} else {
err = phy_write_mmd(phydev, DP83812_DEVADDR, MII_DP83812_SGMII_CTRL,
(~DP83812_SGMII_EN & value));
}
if (err < 0)
return err;
return 0;
}
static int dp83812_ack_interrupt(struct phy_device *phydev)
{
int err;
err = phy_read(phydev, MII_DP83812_INT_STAT1);
if (err < 0)
return err;
err = phy_read(phydev, MII_DP83812_INT_STAT2);
if (err < 0)
return err;
err = phy_read(phydev, MII_DP83812_INT_STAT3);
if (err < 0)
return err;
return 0;
}
static int dp83812_config_intr(struct phy_device *phydev)
{
int misr_status, err;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
misr_status = phy_read(phydev, MII_DP83812_INT_STAT1);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83812_ESD_EVENT_INT_EN |
DP83812_LINK_STAT_INT_EN |
DP83812_ENERGY_DET_INT_EN |
DP83812_LINK_QUAL_INT_EN);
err = phy_write(phydev, MII_DP83812_INT_STAT1, misr_status);
if (err < 0)
return err;
misr_status = phy_read(phydev, MII_DP83812_INT_STAT2);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83812_SLEEP_MODE_INT_EN |
DP83812_OVERTEMP_INT_EN |
DP83812_OVERVOLTAGE_INT_EN |
DP83812_UNDERVOLTAGE_INT_EN);
err = phy_write(phydev, MII_DP83812_INT_STAT2, misr_status);
if (err < 0)
return err;
misr_status = phy_read(phydev, MII_DP83812_INT_STAT3);
if (misr_status < 0)
return misr_status;
misr_status |= (DP83812_LPS_INT_EN |
DP83812_WAKE_REQ_INT_EN |
DP83811_NO_FRAME_INT_EN |
DP83811_POR_DONE_INT_EN);
err = phy_write(phydev, MII_DP83812_INT_STAT3, misr_status);
} else {
err = phy_write(phydev, MII_DP83812_INT_STAT1, 0);
if (err < 0)
return err;
err = phy_write(phydev, MII_DP83812_INT_STAT2, 0);
if (err < 0)
return err;
err = phy_write(phydev, MII_DP83812_INT_STAT3, 0);
}
return err;
}
#if 0
static irqreturn_t dp83812_handle_interrupt(struct phy_device *phydev)
{
bool trigger_machine = false;
int irq_status;
/* The INT_STAT registers 1, 2 and 3 are holding the interrupt status
* in the upper half (15:8), while the lower half (7:0) is used for
* controlling the interrupt enable state of those individual interrupt
* sources. To determine the possible interrupt sources, just read the
* INT_STAT* register and use it directly to know which interrupts have
* been enabled previously or not.
*/
irq_status = phy_read(phydev, MII_DP83812_INT_STAT1);
if (irq_status < 0) {
phy_error(phydev);
return IRQ_NONE;
}
if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
trigger_machine = true;
irq_status = phy_read(phydev, MII_DP83812_INT_STAT2);
if (irq_status < 0) {
phy_error(phydev);
return IRQ_NONE;
}
if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
trigger_machine = true;
irq_status = phy_read(phydev, MII_DP83812_INT_STAT3);
if (irq_status < 0) {
phy_error(phydev);
return IRQ_NONE;
}
if (irq_status & ((irq_status & GENMASK(7, 0)) << 8))
trigger_machine = true;
if (!trigger_machine)
return IRQ_NONE;
phy_trigger_machine(phydev);
return IRQ_HANDLED;
}
#endif
static int dp83812_config_aneg(struct phy_device *phydev)
{
int value, err;
if (phydev->interface == PHY_INTERFACE_MODE_SGMII) {
value = phy_read_mmd(phydev, DP83812_DEVADDR, MII_DP83812_SGMII_CTRL);
if (phydev->autoneg == AUTONEG_ENABLE) {
err = phy_write_mmd(phydev, DP83812_DEVADDR,
MII_DP83812_SGMII_CTRL,
(DP83812_SGMII_AUTO_NEG_EN | value));
if (err < 0)
return err;
} else {
err = phy_write_mmd(phydev, DP83812_DEVADDR,
MII_DP83812_SGMII_CTRL,
(~DP83812_SGMII_AUTO_NEG_EN & value));
if (err < 0)
return err;
}
}
return genphy_config_aneg(phydev);
}
static int dp83812_probe(struct phy_device *phydev)
{
struct dp83812_private *dp83812;
int ret;
dp83812 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83812), GFP_KERNEL);
if (!dp83812)
return -ENOMEM;
ret = dp83812_read_straps(phydev);
if (ret)
return ret;
switch (phydev->phy_id) {
case DP83TC812_CS1_0_PHY_ID:
dp83812->chip = DP83812_CS1;
break;
case DP83TC812_CS2_0_PHY_ID:
dp83812->chip = DP83812_CS2;
break;
case DP83TC813_CS2_0_PHY_ID:
dp83812->chip = DP83813_CS2;
break;
case DP83TC814_CS2_0_PHY_ID:
dp83812->chip = DP83814_CS2;
break;
default:
return -EINVAL;
};
/* vikram : above code added to switch between different phy ids */
return dp83812_config_init(phydev);
}
#define DP83812_PHY_DRIVER(_id, _name) \
{ \
PHY_ID_MATCH_EXACT(_id), \
.name = (_name), \
.probe = dp83812_probe, \
/* PHY_BASIC_FEATURES */ \
.soft_reset = dp83812_phy_reset, \
.config_init = dp83812_config_init, \
.config_aneg = dp83812_config_aneg, \
.ack_interrupt = dp83812_ack_interrupt, \
/*if 0 \
.handle_interrupt = dp83812_handle_interrupt, \
#endif */ \
.config_intr = dp83812_config_intr, \
.suspend = genphy_suspend, \
.resume = genphy_resume, \
}
static struct phy_driver dp83812_driver[] = {
DP83812_PHY_DRIVER(DP83TC812_CS1_0_PHY_ID, "TI DP83TC812CS1.0"),
DP83812_PHY_DRIVER(DP83TC812_CS2_0_PHY_ID, "TI DP83TC812CS2.0"),
DP83812_PHY_DRIVER(DP83TC813_CS2_0_PHY_ID, "TI DP83TC813CS2.0"),
DP83812_PHY_DRIVER(DP83TC814_CS2_0_PHY_ID, "TI DP83TC814CS2.0"),
};
module_phy_driver(dp83812_driver);
static struct mdio_device_id __maybe_unused dp83812_tbl[] = {
{ PHY_ID_MATCH_EXACT(DP83TC812_CS1_0_PHY_ID) },
{ PHY_ID_MATCH_EXACT(DP83TC812_CS2_0_PHY_ID) },
{ PHY_ID_MATCH_EXACT(DP83TC813_CS2_0_PHY_ID) },
{ PHY_ID_MATCH_EXACT(DP83TC814_CS2_0_PHY_ID) },
{ },
};
MODULE_DESCRIPTION("Texas Instruments DP83TC812 PHY driver");
MODULE_AUTHOR("Hari Nagalla <hnagalla@ti.com");
MODULE_LICENSE("GPL");
if you have any suggestions and methods, please do not hesitate to advise, look forward to your reply!