Part Number: NS16C2752
Tool/software:
Hi,
I have any question.
1, When resetting by the MR pin, which timing is correct when/TXRDYx goes from High to Low?
a) At the same time as resetting by the MR pin
b) x sec after resetting by the MR pin. If there is a formula or specification for x sec, please tell me.
2, Which is correct about the relationship between power-on reset and MR reset?
a) When both resets are released, IC releases reset.
b) When one reset is released, IC releases reset.
3, What is the voltage threshold value at which power-on reset is released?
Best Regards,
Nishie