Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83561-SP: Power-on diagram clarification

Part Number: DP83561-SP

Tool/software:

Hello, in figure 6-1 of the DP83561-SP datasheet, for the power up timing, is T1 with respect to the VDD rail coming up or with respect to clock edge?

We were not certain given the parameter description for T1 is last supply power rail ramp to RESET_N, but in the drawing, it appears to be going to the clock edge.

Is this assuming rails ramp up and stable clock provided followed by 200ms from the first stable clock edge?

 

Secondly, the T3 time for the straps to latch is specified only at nominal to 200ms. Is there a max time we should be waiting before attempting to use these dual pins?

Thank you!

  • Hi Tijana,

    I think the datasheet might be confusing. The mean time we are referring to for T3 is the minimum time we need to wait after power up for the Dual pins enable. There is no requirement for the maximum waiting time after power up.

    --

    Regards,

    Hillman Lin