Part Number: ONET1101L
Tool/software:
We are using Onet1101L for modulation of laser diode with a built-in photo detector. Our circuit design is more or less a copy of the reference design in the data sheet. We operate in APC mode with a bias current around 45mA, and it works perfectly although our modulation frequency is only 40MHz (on-off modulation). The only problem is that we cannot get the laser safety feature to work. When FLTEN=1 the driver shuts off the bias and modulation current immediately and the FLT-pin goes high. When setting FLTEN =0, the FLT-pin goes low and the bias and modulation current goes back on immediately .
According to the datasheet the ONET1101L the laser safety feature will react on the following conditions:
1. Voltage at MONB exceeds the voltage at RZTC (1.16 V).
In our case V_MONB=0.5V and V_RZTC=1.147V. Hence this should not trigger a fault
2. Photodiode current exceeds 150% of its set value.
What is photo current set value? Is it max value defined by PDRNG? We use PDRNG1&2=00 (i.e max photo current 0.77mA.
In our case V_MONP=0.15V => I_PD = (0.15V/5K)/50% =0.06mA. Can this be the case of the fault?
3. Bias control DAC drops in value by more than 50% in one step.
What does this mean and how can we check this?