Part Number: TCAN4550
Tool/software:
Hi TEAM,
Please help on below two question, thanks!
1. I am configuring TCAN4550 now, and I do not intend to use the interrupt request bit to send or receive data. If the MCU polls to send and receive data, do I need to configure the interrupt of TCAN4550?
2. The value of the 0X000C register is 0x0800000C, the value of the 0x0820 register is 0x00010089, and the value of the 0x0824 register is 0x08010000. What are the possible reasons for these errors?
Best,
Well