This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB962-Q1: display misalignment

Part Number: DS90UB962-Q1

Tool/software:

OEM:SAIC

APP Diagram:

Issue: only camera 4: display misalignment:(two images seams at the front and back of the car)

have done:

1、soft reset:0x01(useless)

2、hardware reset: Power down--power up--inti reg--(useless)

Repetition rate: 1\250

log:

The investigation of the system log found that there were a large number of frame back logs for the same stream _ id.
The application side thinks no flow timeout, and the restart mechanism restarts the entire camera frame

camera-933-963-soc(system diagram): sorry for I have no time to redraw a diagram in Eng, this diagram is from China customer;

Thanks a lot

BR.

Violet