Part Number: SN75LVPE5412
Other Parts Discussed in Thread: DS160PR410
Tool/software:
hello
We are comparing and evaluating ds160pr410 and SN75LVPE5412. We made an evaluation board with the same input and output loss and evaluated it.
We set the DS160 EQ index to 29 and the SN75 EQ index to 19 (both DC gain set to 0dB).
At 8GHz, the gain of DS160PR410 is about 2.5dB higher than that of SN75LVPE5412. The frequency characteristics of SN75LVPE5412 (EQ index 19) are similar to those of DS160PR410 (EQ index 23-24).
Is this the correct result?
The data sheet shows that both have a similar gain of 17dB at 8GHz, so I'm asking.