Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB926Q-Q1: Blue screen

Part Number: DS90UB926Q-Q1

Tool/software:

Hi team,

My customer uses 949-926-DLP to output a 800*480 display signal.

They tested DLP BIST mode and everything was normal.

Then they enabled 949 white pattern and found the screen was a bit blue.

They want to know if it is caused by white balance and how to fix it.

Now they are testing 926 pattern and I will update the result tomorrow.

Regards,

Peter 

  • Hi Peter,

    Are you using color bars? Furthermore, please update us with the results of the 926 pattern. It will help with narrowing down where the issue is. 

    Thanks,

    Esther

  • Hi Esther,

    Their display module is DLP module which cannot tolerate large PCLK mismatch.

    926 pattern could only output 33.3MHz PCLK and DLP needs 31.5MHz, so DLP output nothing when in 926 pattern mode.

    Could you ask your colleagues which has experience on FPD-link pairing DLP system?

    Regards,

    Peter

  • Hi Peter,

    I have several questions:

    1) Which type of RGB format are you using?

    2) Can you provide a picture of a "blue" display? 

    There are several options that you can try:

    1) Use an external oscillator on Pin 5 of the 926 rated at 31.5 MHz and try 926 PATGEN with internal timings/external clock. 

    2) Swap out the display with one that can accept the 33.3 MHz PCLK and try 926 PATGEN again. 

    3) Run the 949 PATGEN with a different display with no other changes. 

    Let us know the results of any of these options.

    Thanks,

    Esther

  • Hi Esther,

    1) Which type of RGB format are you using?

    RGB888.

    2) Can you provide a picture of a "blue" display? 

    I will upload a video later.

    1) Use an external oscillator on Pin 5 of the 926 rated at 31.5 MHz and try 926 PATGEN with internal timings/external clock. 

    This is not possible because they did not reserve oscillator on their board.

    2) Swap out the display with one that can accept the 33.3 MHz PCLK and try 926 PATGEN again. 

    Customer also said it is not possible because their board is specialized made for DLP module. 

    3) Run the 949 PATGEN with a different display with no other changes. 

    Not possible, the same reason as 2).

    We are trying to output a red/green pattern and capture the signal on blue lane. What should the blue signal lane(pin19, B0) be when 926 outputs a red/green pattern?

    Regards,

    Peter

  • Hi Esther,

    Please check the video below.

    Regards,

    Peter

  • Hi Peter,

    Are you using color bars?

    Can you please try using color bars for 949 PATGEN and send a video of the result? It will give us a better idea on the behavior we're seeing, as opposed to using a solid color pattern.

    BR,

    Esther

  • Hi Esther,

    Please check their display.

    They can see abnormal blue lines in the display.

    Regards,

    Peter

  • Hi Peter,

    Thank you for the pictures. To help narrow down the cause of this distortion, what PCLK are you using when you do 949 PATGEN? It could be an issue with the PCLK tolerance of the DLP display, similar to the 926 case. 

    BR,

    Esther