Part Number: TUSB320
Tool/software:
Hi,
We are targeting the TUSB320HAIRWBR for a an UFP that can operate using USB-C default (500 mA) or mid-range (1.5A) 5V power.
Will this device operate correctly if it is plugged into a charger or DFP that supports USB-PD? Specifically, if the DFP starts sending USB-PD messages over the CC lines, will the TUSB320HAIRWBR ignore the response and not be confused by the lines toggling will monitoring the Rd current (the USB-C power contract mechanism)?
Thanks,
Mike