Part Number: VAR-3P-SOM-AM62
Tool/software:
Hi everyone,
i have the VAR-SOM-AM625 SoM and i want to use the PTP Protocoll. When i check the MAC network interface if it supports PTP i get the following:
Time stamping parameters for eth0:
Capabilities:
hardware-transmit
software-transmit
hardware-receive
software-receive
software-system-clock
hardware-raw-clock
PTP Hardware Clock: 0
Hardware Transmit Timestamp Modes:
off
on
Hardware Receive Filter Modes:
none
all
I did not get any specific output wehter it supports hardware of software time stamping and i know it supports both.
I have allready activated the CPTC Module in the Kernel und it is active.
So whay i got this and what should i do?
Thank you
Best regards
Zain