Part Number: DS90LVRA2-Q1
Tool/software:
1. The Absolute Maximum Ratings of DS90LVRA2-Q1 allow for a VCC of 0V to 4V. I understand that if I set VCC to a voltage not within the range of one of the three modes lists (1.8V, 2.5V, 3.3V) that the output specifications listed will then not apply. But would there be any other reason not to do this? In my application I have a supply of 3.0V+/-10% and the output level is not critical. But I need to know that the device will otherwise function as expected.
2. The input thresholds are specified for VCC from 1.62V to 3.6V, which appears okay. It mentions Vib from -4V to 5V. What does Vib refer to?