Other Parts Discussed in Thread: DS100MB203
Tool/software:
We are using this component in designing a system that:
- Repeats an input signal to two outputs. (this device has 4 ports to support quad lanes)
- Target is to be able to repeat 10Ghz signals.
Few things I wanted to know.
1. How long is the foretasted availability of the component (we are looking for at least next 10 years)
2. Does this device support SFI signal (10 Gbps).
3. while checking some forums here, it looks like the buffer is not suitable for 10GBASE CR standard? --> passive DAC cable
But it complies with the SR standard , is this observation correct?
Some forum Reference