Part Number: TUSB8043A
Other Parts Discussed in Thread: AM67
Tool/software:
Hi,
two questions:
(1) we're planning to have this USB hub on one of our boards which has two USB2.0 and two USB3.2 ports. Thus, some of the ports of the hub are used in USB2 mode only. I've seen there are some configuration bits to disable the USB3.2 port (USB2_ONLY in register 26h). Do we need to set this bit? If not, what's the purpose of it?
(2) According to the datasheet, there is an OTP configuartion. Is there any documention how to program/configure the USB hub over the upstream USB connection? We don't want to attach an external configuration EEPROM to save BOM costs (and prevent any preprogrammed parts) thus we'd like to use the internal OTP.
Best regards,
Michael Walle