Part Number: SN65DSI86EVM
Tool/software:
Hi TI team,
Verify that the schematic is supported

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Here is the schematic review.
SN65DSI86_Schematic_Review(10_7_2024).pdf
Additionally, a sample schematic can be found in the DSI86EVM users guide: https://www.ti.com/lit/pdf/sllu204
I have provided a sample layout using the DSI86 here. Keep in mind this is the EVM design and thus has a DP connector rather than an embedded connector.
Please implement the aux as follows with the optional pull up and pull down resistors:

Hi,
Here is the schematic review.
Additionally, a sample schematic can be found in the DSI86EVM users guide:
I have provided a sample layout using the DSI86 here. Keep in mind this is the EVM design and thus has a DP connector rather than an embedded connector.
Please implement the aux as follows with the optional pull up and pull down resistors:

What exactly is the flash screen?
Have you set up the registers correctly? Does the same issue happen with the color bar pattern?
Please re config the register using the DSI tuner tool: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1382976/faq-sn65dsi8x-programming-tools?tisearch=e2e-sitesearch&keymatch=sn65dsi84#
The display has been turned on and the screen is functioning normally, but there is occasional flickering when the projector is first turned on, and there is also occasional flickering when the projector is woken from sleep mode.
Hi,
For the occasional flickering when the projector is first turned on, are you following the power-on sequence as shown in section 8.4.2 of the DSI86 datasheet, In particular, this part of the sequence?
For the sleep mode, are you putting the DSI86 into the Suspend mode as well?
Thanks
David