Part Number: TRSF3232E
Other Parts Discussed in Thread: SN65C3232E, MAX3232E, TRS3232E
Tool/software:
The part number TRSF3232E is declared as a 1Mbit/s RS232 transceiver, but at paragraph 9.2.1 (Design Requirements) is indicated that "• Maximum recommended bit rate is 250 kbites".
In data sheet of the similar P/N SN65C3232E (now not suggested for new designs) at the same paragraph is written "• Maximum recommended bit rate is 1 Mbps".
Is the first indication a mistake?
Can I use the TRSF3232E as a replacement of SN65C3232E also at 1Mbps?