Part Number: TLIN1021A-Q1
Tool/software:
Hello!
When using the TLIN1021ADRBRQ1 chip, we tested the SAE2602-1 standard and had the following requirements:
VECU=8V,The commander-node must transition from waking to not waking in response to the wake- up message wher 4.8 V ≥Recessive LIN bus voltage ≥ 3.29 V.
We use it as a slave mode.
However, according to the manual, only the minimum High level given to LIN is 0.6xVSUP=4.8V. We have measured that it fails at 6.09V, which is within the scope of the manual but does not meet the SAE2602 standard and needs to fail between 3.29V-4.8V.