Part Number: TCA9548A-Q1
Tool/software:
can set I2C target address same as the device I2C address?
example: TCA9548 0X74,target address also set as 0X74?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9548A-Q1
Tool/software:
can set I2C target address same as the device I2C address?
example: TCA9548 0X74,target address also set as 0X74?
It appears there is a misunderstanding. Please show your system architecture with all I²C addresses.
When you want to access the TCA9548A-Q1's control register, then you have to use address 0x74 (or whatever is configured with A0/A1/A2).
When you want to access another device, then you have to use the address of that device (which must be different from 0x74).
Hello Zhou,
Like Clemens said the address of different devices on the i2c bus must be different for proper communication.
If not you will run into something called address conflict.
Check out this App note which talks about several ways the problem can be solved.
Please let me know what you think after reading this and we can look into a solution for this further.
Regards,
kameron
The addresses 0x70 and 0x74 are already used by the two switches. When the master sends a command to address 0x70 and 0x74, then one of the switches will act on it. So it is not allowed for another device on any of the buses 1.1…1.8 or 2.1…2.8 to have address 0x70 or 0x74. All other addresses are allowed.
Multiple devices on those channels can have the same address, as long as only one of those channels is enabled at the same time.