Part Number: TL16C752C
Tool/software:
Hi team,
I am running at 512kbps and it works fine when transmitting but gradually loses the INT signal when receiving.
Are there any conditions under which the INT signal stops being generated?
When the INT signal is gradually lost, the timing of INT signal generation shifts.
At first, the INT signal is generated before the RX start bit, but it is gradually shifted so that it is generated after the RX start bit, and finally the signal is no longer output.
The part being checked is INTA.
I assume that you are reading the received 1 bit with 16 bit oversampling.
In this case, I would like to know what bit is being read.
Best Regards,
Ryu.