Other Parts Discussed in Thread: TCAN24XXEVM
Tool/software:
"The VCC1 pin is capable of sinking either 10μA or 1000μA of current depending upon the register setting VCC1_SINK and is active by default. The current sink can be disabled by setting the register bit VCC1_SINK_DIS."
Yes, I understand the VCC1_SINK_DIS is a switch of VCC1 sinking current and VCC1_SINK is used to selected the max VCC1 sinking current 10uA or 1000uA.
My Question:
1. I keep the VCC1_SINK_DIS = enable and VCC1_SINK = 1000uA. What are the influences of this configuration?
2. What condition I need to change the VCC1_SINK from 1000uA to 10uA?
3. What condition I need to change the VCC1_SINK_DIS from enable to disable?