Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P82B715: Application issues of chips

Part Number: P82B715

Tool/software:

1.8V I2C
But in the absence of communication, the voltage of I2C is around 2.2V, and during communication, I2C will drop to around 1.8V
So the overall waveform presents a stepped shape
Under normal circumstances, it should be a stable voltage. What causes these steps?How to solve this problem? 

The platform uses 1.8V I2C, so it's not easy to change to 3.3V temporarily

The schematic diagram is as follows

The application of chips is similar to this situation

There are two boards
Two boards are connected via I2C, with a wire length of 1.2M
A structure similar to this