Part Number: TCA9517-Q1
Tool/software:
hi TI expert
We use a structure similar to the one shown in the figure to design an MCU with 3.3V, which is converted to a 1.8V level through LEVELSHIFT. Occasional MCU I2C card dead situation, test BUS-B with SCL at high level 3.3V and SDA at low level 0.5V when stuck; The SCL of BUS-A is at a high level of 1.8V, while SDA is at a low level of approximately 0V.
(1) May I ask what circumstances could lead to this scenario?
(2) We tried to turn down and up the power supply of VCCA, but the bus still froze. Can the SDA of BUS-B still output a low level of 0.5V after VCCA is powered off?
thank you