Part Number: LMH0302
Tool/software:
Hi
We have some questions related to the 3G SDI (LMH0302) functionality:
- Can we use only one of the BNC outputs, either SDO+ or SDO-? If so, which one, SDO+ or SDO-, is recommended for use as the BNC output?
- Do SDO+ and SDO- need to be used simultaneously for output?
Can I use only one BNC Output? Or must I use two BNC Outputs at the same time?

If only one channel is used, which BNC Output channel is recommended?