Part Number: DS125BR401
Tool/software:
dears,
My customer used SMBus Master Mode (ENSMB = float) to load register data from external EEPROM (AT24C02C; EEPROM address is 0xA0, 3 repeater AD[3:0] is 0XB0)to DS125BR401,
, but it failed to load data from EEPROM when power up; however, if reset the registers by setting the bit 6 (Reset Registers) of 0X07 register (Digital Reset and Control), the data may be loaded from the external EEPROM.
i noticed that there is a pin, READ_EN, it is said in the datasheet,: " When using an External EEPROM, a transition of READ_EN pin from high to low starts LVCMOS the load from the external EEPROM", is it also necessary for the Master Mode? the datasheet does not require READ_EN pin high-to-Low transition in master mode work sequence (9.5.2 SMBUS Master Mode).
when does DS125BR401 load the data from external EEPROM? will the power quality affect the data loading?
the customer set the mode at 10G-KR, they also noticed that the 2 bits, 0x26[6:5] (MODE_DET Status), may change between 11 and 00, is it abnormal? As the datasheet says these 2 bit "Only functions when MODE Pin = Automatic", could we just ignore them?
please help to have a look of the issues.
thanks a lot!