Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401: About TFP401

Part Number: TFP401

Tool/software:

The TFP401 supports the following resolutions. ...

1,VGA :640*480,60Hz

2,SVGA  :800*600,60Hz

3,XGA    :1024*768,60Hz

4,WXGA :1280*768,60Hz

5,QUAD-VGA :1280*960,60Hz

6,SXGA :1280*1024,60Hz

7,FHD  :1920*1080,60Hz

  • The TFP401 can support any pixel rate lower than 165MHz.

    pixel rate can be estimated as follows: Vactive * Hactive * 1.3 * Refresh rate

    ex) 1920 * 1080 * 1.3 * 60 = 161.74 MHz. 

    All resolutions lower than this are supported.

    The TFP401 support all the resolution you are looking to use.