Part Number: TCAN3414
Tool/software:
Hi, I have a simple question. I use the TCAN3414 in my system. Which is a 3v3 CAN driver. Now, we need (or do we?) CAN ground. Is this compatible with 5V drivers? If I'm right, the idle bus voltage of 3v3 and 5v CAN drivers differ. With the 5V ones being 2.5V and the 3v3 ones being 1.65v. Am I right that this is going to possibly cause problems or add extra current flow? Nothing seems to be written about this topic.