This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EQ50F100: Thermal Characteristics

Part Number: EQ50F100

Tool/software:

Hello,

I'm in the process of choosing an Equaliser where I require x5 channels supporting a data rate up to 3.2Gbps. In my initial search this part appeared to be a potential contender, though the datasheet lacked the Maximum Operating Junction Temperature.

I wonder if this attribute can be provided, please?

In terms of actually specifying a part, I'd also invite any recommendations you may have. My requirements are below:

  • Data rate = up to 3.3Gbps
  • Minimum Storage Temperature = -54 degrees celsius
  • Max. Operating Temperature = ideally above 100 degrees celsius. (85 can be considered if the Max. Operating Junction Temperature for the part is also specified/ available.)
  • Number of channels = ideally x5, though I'm happy to feature multiple instances of the same part if the above thermal attributes are available for concerned parts/ can be provided.

Many thanks in advance!

Pete.