Part Number: MAX3232E
Tool/software:
If unused channel of TX and RX needed external pull up and pull down for or it has internal pull up and pull down for it. Or it OK to use it as no connect for the unused pin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MAX3232E
Tool/software:
If unused channel of TX and RX needed external pull up and pull down for or it has internal pull up and pull down for it. Or it OK to use it as no connect for the unused pin
Hi Clemens
Din1 ,Rin1 can be left open or need to be pulled up with resistor or pulled down with resistor
Is there amy issue if left open Din1, Rin1, Dout 1, Rout1
when i checked the data sheet Rin1 has internal pull down of 5K .is this the same case of DIN1
Hi Rony,
The unused RIN and DIN pins cannot be floating. It is best practice to tie RIN and DIN to ground with a 3 to 5K resistor if not in use. DOUT and ROUT pins can be left floating if not in use.
Regards,
Ethan