Other Parts Discussed in Thread: TUSB320,
Tool/software:
the scenior is : Tablet -> USB micro wire -> TUSB320 -> typeC adaptor with TYPE A connector -> USB flash
connected 5V power supply to J5 DC INPUT
DIP switchs SW1 is set to DRP mode(SW1.1~1.8= 10000000).
I adapt the type C hub with USB flash while D4(320_ID) bringup.
but tablet still can't access USB flash.
is it any suggestion?