This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TD510E-EVM: DP83TD510E-EVM

Expert 1035 points

Part Number: DP83TD510E-EVM

Tool/software:

In SPE(Single pair Ethernet) testings on CAT6 cable of 8ohms resistance per 100m ,its working up to 600m and on power cable of 1.5sq mm 10 conductor cable its working only 300m and resistance value is 2 ohms per 100m.

our impedance matching circuit is 100ohms.
operating Phy in 2.4v p2p.

what are the modifications that we need to do in order to achieve 2km or increase the range of distance?