Part Number: DP83822I
Tool/software:
We're having intermittent issue with the Ethernet XCVR. Applied 25 MHZ oscillator on pin 23. The PN of the Ethernet XCVR is DP83822IRHBT.
Pins 2 (TX_CLK), 23 (XI) and 25 (RX_CLK) probed with an oscilloscope. In the failed state no clocks were observed on pins 2 and 25. The oscillator input on pin 23 was present and measured at 25 MHz’s. When the unit was probed in the working state pins 2 (TX_CLK), 23 (XI) and 25 (RX_CLK ) displayed good clocks. At this point we believe the issue is within the TI Ethernet transceiver.