Part Number: DP83826E
Other Parts Discussed in Thread: STRIKE
Tool/software:
Hi, I am looking for support to address ESD issue on the Ethernet PHY DP83826E. This happen when the board is supply by PoE and an ESD discharged arrived by an other connector referenced to the ground of the board. The PoE signals are referenced to the PoE ground which is himself separated from the main ground of the board.
The pins 17, 29 & 30 are short circuited when a 8kV is applied on the other connector. The ESD gun is referenced to an earth reference that is the same as the PoE supply.
Do you have any idea about what is happening and what could be the solution to support the ESD discharge ?