Part Number: DP83849I
Other Parts Discussed in Thread: DP83869
Tool/software:
Hi,
I need help in finding a network cable tester/diagnostic IC that can acheive the following tests:
- Wire Map Test - Checks for proper pin configurations and identifies wiring errors such as cross-wiring, miswires, and split pairs.
- Continuity Test - Verifies that each conductor in the cable is complete and not broken, ensuring the physical integrity of the cable.
- Cable Length Test - Measures the length of the cable and helps identify if the cable length is within the specifications required for reliable communication. A TDR method would be required, I think.
- Crosstalk Test - Measures the interference between pairs within the cable
- PoE Test - Checks for the presence of PoE on the cable and measures the voltage, verifying if the power levels meet the device requirements.
- IP Configuration Test - Verifies the correct assignment of IP addresses to devices by DHCP and checks for static IP configuration errors
I think multiple chips would be required and some analog switches would be needed. Any help in this regard will be very helpful for me.