Part Number: TFP410
Tool/software:
Hello,
Could you tell me the detailed wiring conditions for board design?
The following was stated in the application note (SLLA135):
- recommended impedance is 50Ω
- trace spacing is 5 times the height
Are there any specified or recommended values for the following conditions?
- allowing Number of vias
- allowed Length of via stubs
- maximum length limit
- trace length matching between P/N differential pair
- total length matching tx pair
Regards.