Part Number: TCAN1044A-Q1
Tool/software:
In the TCAN1044A-Q1 and SN1044-Q1 chip manuals, the ESD section does not explicitly write about the discharge network in power on and power off mode. The SN1044 chip manual only writes the contact discharge network in power-off mode (150pF, 330Ω), and does not write the discharge network in power mode. Discharge networks are not written in the TCAN1044 chip manual. Our company would like to know more clearly the ESD discharge network and discharge level of TCAN1044 and SN1044.Thanks.