Part Number: TUSB522P
Tool/software:
I am looking at the datasheet for the TUSB522P and see that the OS, EN_RXD, EQ and DE pads are connected to 47kOhm resistors and ground and 3.3 voltage in the Embedded Host Application. I believe that the only pins that are connected to the USB connector are the high speed signals, Voltage and Ground, but I was wondering if anything needs to be connected to the OS, EN_RXD, EQ and DE pads. Do they need to be connected to an outside voltage source?
Also, I noticed that RX2N/P has either no capacitor or a 330 nF capacitor. However, I have a "Host" on either side of my assembly and was wondering if that would mean that the 100nF capacitors should be on all Tx/Rx lines? I have included an image of my simplified assembly.
Best, Arron